Schneider Electric - Electrical Distribution and Automation and Control

Voltage drop

Voltage drop

This is an excerpt from the sizing and protection of conductors chapter in The Electrical Installation Guide. You can download this excerpt which looks at the determination of voltage drop by simply downloading the sizing and protection of conductors chapter by clicking here.

Determination of voltage drop

The impedance of circuit conductors is low but not negligible: when carrying load current there is a voltage drop between the origin of the circuit and the load terminals. The correct operation of a load (a motor, lighting circuit, etc.) depends on the voltage at its terminals being maintained at a value close to its rated value. It is necessary therefore to determine the circuit conductors such that at full-load current, the load terminal voltage is maintained within the limits required for correct performance.

This section deals with methods of determining voltage drops, in order to check that:

Maximum voltage drop

Maximum allowable voltage-drop vary from one country to another. Typical values for
LV installations are given below in Figure G25.

voltage drop

These voltage-drop limits refer to normal steady-state operating conditions and do not apply at times of motor starting, simultaneous switching (by chance) of several loads, etc. as mentioned in Chapter A Sub-clause 4.3 (factor of simultaneity, etc.). When voltage drops exceed the values shown in Figure G25, larger cables (wires)
must be used to correct the condition.

The value of 8%, while permitted, can lead to problems for motor loads; for example:

maximum voltage drop

Calculation of voltage drop in steady load conditions

Use of formulae

Figure G27 below gives formulae commonly used to calculate voltage drop in a given circuit per kilometre of length.

If:

voltage drop calculation

Note: R is negligible above a c.s.a. of 500 mm2

Simplified table

Calculations may be avoided by using Figure G28 next page, which gives, with an adequate approximation, the phase-to-phase voltage drop per km of cable per ampere, in terms of:

Voltage drop in a cable is then given by:
K x IB x L
K is given by the table,
IB is the full-load current in amps,
L is the length of cable in km.

The column motor power “cos sign = 0.35” of Figure G28 may be used to compute the voltage drop occurring during the start-up period of a motor (see example no. 1 after the Figure G28).

voltage drop table

*You might also find this voltage calculator from NoOutage useful.


back to electrical installation guide  Back to Electrical Installation Guide
2009 Edition