logo Schneider Electric  and Brand Tag
Engineering resources

Characteristics of particular sources and loads

Most industrial and large commercial electrical installations include certain important loads for which a power supply must be maintained, in the event that the utility electrical supply fails:
Electrical Installation guideEither, because safety systems are involved (emergency lighting, automatic fireprotection equipment, smoke dispersal fans, alarms and signalization, and so on.) or,
Electrical Installation guideBecause it concerns priority circuits, such as certain equipment, the stoppage of which would entail a loss of production, or the destruction of a machine tool, etc.

One of the current means of maintaining a supply to the so-called "priority" loads, in the event that other sources fail, is to install a diesel generator set connected, via a change-over switch, to an emergency-power standby switchboard, from which the priority services are fed.


Function Block Library EIG-N-sources-loads-1.pdf


icone  Back to Electrical Installation Guide

2009 Edition
visuel automation solution guide and electrical installation guide