logo Schneider Electric  and Brand Tag
Engineering resources

Protection against voltage surges in LV

A voltage surge is a voltage impulse or wave which is superposed on the rated network voltage. Lightning comes from the discharge of electrical charges accumulated in the cumulo-nimbus clouds which form a capacitor with the ground.

Direct or indirect lightning strokes can damage electrical equipment at a distance of several kilometers. Operating voltage surges, transient and industrial frequency over-voltage can also produce the same consequences.The effects are described in this chapter such as overvoltage protection devices and the way to choose the appropiated one. Implementation rules are given respecting installation standards for primary and secondary protection devices.


Function Block Library EIG-J-protection-voltage-surges.pdf


icone  Back to Electrical Installation Guide

2009 Edition
visuel automation solution guide and electrical installation guide