logo Schneider Electric  and Brand Tag
Engineering resources

Sizing and protection of conductors

Component parts of an electric circuit and its protection are determined such that all normal and abnormal operating conditions are satisfied. Each circuit is then studied in detail.
From the rated currents of the loads, the level of short-circuit current, and the type of protective device, the cross-sectional area of circuit conductors can be determined, taking into account the nature of the cableways and their influence on the current rating of conductors.
Before adopting the conductor size indicated above, the following requirements must be satisfied:
Electrical Installation guideThe voltage drop complies with the relevant standard
Electrical Installation guideMotor starting is satisfactory
Electrical Installation guideProtection against electric shock is assured

The short-circuit current Isc is then determined, and the thermal and electrodynamic withstand capability of the circuit is checked. These calculations may indicate that it is necessary to use a conductor size larger than the size originally chosen.


Function Block Library EIG-G-sizing-protection-conductors.pdf

 

Prewiew two pages of this chapter here: voltage drop.


icone  Back to Electrical Installation Guide

2009 Edition
visuel automation solution guide and electrical installation guide