logo Schneider Electric  and Brand Tag
Engineering resources

Protection against electric shocks

When a current exceeding 30 mA passes through a part of a human body, the person concerned is in serious danger if the current is not interrupted in a very short time.
The protection of persons against electric shock in LV installations must be provided in conformity with appropriate national standards statutory regulations, codes of practice, official guides and circulars etc.
Relevant IEC standards include: IEC 60364, IEC 60479 series, IEC 61008, IEC 61009 and IEC 60947-2.


Function Block Library EIG-F-protection-electrical-shocks.pdf


icone  Back to Electrical Installation Guide

2009 Edition
visuel automation solution guide and electrical installation guide