logo Schneider Electric  and Brand Tag
Engineering resources

Connection to the MV utility distribution network

At present there is no international agreement on precise limits to define "medium" voltage.
Voltage levels which are designated as "medium" in some countries are referred to as "medium" in others.
In this chapter, distribution networks which operate at voltages of 1,000 V or less are referred to as Low-Voltage systems, while systems of power distribution which require one stage of stepdown voltage transformation, in order to feed into low voltage networks, will be referred to as Medium- Voltage systems.
For economic and technical reasons the nominal voltage of medium-voltage distribution systems, as defined above, seldom exceeds 35 kV.


Function Block Library EIG-B-connection-MV-network.pdf


icone  Back to Electrical Installation Guide

2009 Edition
visuel automation solution guide and electrical installation guide