logo Schneider Electric  and Brand Tag
Engineering resources

General rules of electrical installation design

The study of a proposed electrical installation requires an adequate understanding of all governing rules and regulations.
The total power demand can be calculated from the data relative to the location and power of each load, together with the knowledge of the operating modes (steady state demand, starting conditions, non simultaneous operation, etc.)
From these data, the power required from the supply source and (where appropriate) the number of sources necessary for an adequate supply to the installation are readily obtained.
Local information regarding tariff structures is also required to allow the best choice of connection arrangement to the power-supply network, e.g. at medium voltage or low voltage level.


Function Block Library EIG-A-electrical-design.pdf


icone  Back to Electrical Installation Guide

2009 Edition

How to design to both enhance availability and lower eploitation costs...

Power monitoring
Control

Power monitoring and control must be taken into account from the very beginning of the design process

Transparent Ready is a simple, ready to connect solution, which doesn't require a specialist.

More resources
PuceIEC Standards
PuceCENELEC Standards
PuceISO Organization
PuceRoHS Directive
PuceWEEE directive